This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0106: Datasheet, Current

Part Number: TXB0106


Hi Team,

I make a calculation about current consumption.

And i want to know if I understand about TXB0106's datasheet.

In TXB0106 datasheet,

Maximum current is 100mA.

And Electrical Characteristics sheet, there is also current table. It is only use 5uA.

The test condition is TXB0106 not working, right? Because Io is 0 A.

so when i do a calculation about current consumption, I refer to the Maximum current (100mA)?