Part Number: TXB0108
Other Parts Discussed in Thread: TXU0304, TXU0104, TXU0204
Hi,
There are two cases where the initial voltage of the device connected to Ax of TXB0108 must be set to High and Low.
Also, an internal pull-up resistor of 15 kΩ to 30 kΩ is connected to the FPGA.
1. When it is High.
1.1. Is the circuit OK with the image below?
1.2. Which resistance value is better for A and B: 100 kΩ, NC or X kΩ (please tell me your recommended value)?

2. When it is High.
2.1. Is the circuit OK with the image below?
2.2. Which resistance value is better for A and B: 100 kΩ, NC or X kΩ (please tell me your recommended value)?

3. Is it correct that 1.8V is applied to the OE after the Device is power-up?
Best Regards,
Nishie