Other Parts Discussed in Thread: SN74LVC1G17, TLV3201, TLV9030
Dear Team,
Please help review following designs and comment. Thanks.
Schmitt Trigger
Input voltage swing is from 3.6V to 1.2V. It could not be recognized by SN74AUP1T17DCKR when the input voltage is less than 1.2V. Please help review and comment hot to improve to make sure UB4 can recognize and output voltage correctly. Thanks.
UB4
- Supply voltage: 3.3V
 - Original input voltage is 5V to 1.2V and will clamped into 3.6V to 1.2V by Q8
 
Many Thanks,
Jimmy