This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1GX04: XTAL buffer

Part Number: SN74LVC1GX04


Hello~.

I need to pass the clock to two ICs with one XTAL.

So, I found the SN74LVC1GX04 like below.

 

Vcc = 3.3V

XTAL Frequency : 25MHz

I can confirm that the gain of the amplifier of SN74LVC1GX04 is reduced at 25MHz.

In this case, Can 25MHz output be guaranteed normally?

Thank you 

Best regards.

  • In theory, any gain above 0 dB is OK. So with 20 dB at 25 MHz, I expect it to work.

    In practice, the oscillator circuit is an analog circuit and depends on the characteristic of all components. Test with the real circuit; see section 9.2.1 of the datasheet for possible modifications.