Other Parts Discussed in Thread: SN74AHC1G08
Hi Team,
Measuring the output pin of the device, find that the output signal jitter violently when the input signal is normal. The troubleshooting found that the input pin of the buffer, the rising edge of pin3 is relatively slow. The rise time of Pin3 is about 2.6ms.
I want to ask, what is the rise time limit of the input signal for SN74LVC1G08? That is, how many ms does the signal rise time be less than without producing a phenomenon similar to signal jitter?
The schematic:

The test waveform of output signal:

Thanks,
Gust