Part Number: TXU0101
Hi, TXU0101 support team
I want to use under the following condition.
- VCCA=1.8V and VCCB=3.3V
- Rising time of output signal < 50mV/ns
- Uni-direction
Here are some questions;
- There are a pull-down resistor on OE pin and Input A pin as shown in the following diagram. What is these internal resistor value?
- Can OE pin be pulled-up via 10kohm resistor?

Thanks
Tamio