Other Parts Discussed in Thread: SN74LVC1G97
The max current for the SN74LVC1G97 is +/- 24mA when powered with a 5V supply. In my team's application, we are using this logic gate to charge/discharge a small capacitor (in one part of the design this is 1nF) which will exceed this current rating for a short amount of time. We cannot add a current limiting resistor since it would add too much delay to the signal.
Is there any guidance on the pulse current rating for this part?