Part Number: SN74LVC8T245
Other Parts Discussed in Thread: TXU0304, TXU0104, TXU0204
Dear Team,
In my board a processor and a microcontroller are communicating using ethernet interface.This is a mac to mac connection.
The processor is working at 3.3V domain and controller at 5V domain.SN74LVC8T245RHLR is used as the level shifter.
May I know my connections are fine or not.I mean the direction selection of SN74LVC8T245RHLR for RX and TX of RMII.
My PIN mapping is given below.

Schematic is given below.


RMII Signal Descriptions of SAMAD52

Regards
HARI