Part Number: LSF0108
The LSF0108 datasheet section 9.2.4 talks about adding a pullup resistor for operation when Vref_B is less than Vref_A + 0.8V. Please verify the additional pull up resistor is for the B to A direction and would not be required if the translator is used in the A to B direction only.
Also, is there a translator like this (configurable and bidirectional) but with faster edges? I have an application with high capacitive loading and the edges look slow in simulation.
Thank you.