Hi Team,
I want to use this IC in my design to latch an interrupt for 1 second.
The input voltage is 1.8V (and so is the interrupt nominal voltage), and the capacitance graph only goes to 10^6 pF.
I want to use R_L of 200kOhm, and a 10uF cap (10^7 pF) - is there a limit on the C_ext pin for maximaum output capacitance?
Please, advice.
Thanks.