Other Parts Discussed in Thread: SN74LVC1G32, SN74AUP1G32, SN74AHC1G32, SN74AUP1T32, SN74LV1T32
Hi Team,
I see that this device can have a Vcc of up to 3.6V.
for the logic input the recommended operation is 2.7V (Vcc)
can this device work with 3.3V logic input? why dose it is limited to 2.7V?
Do you have a different recommendation?
Best regards.