Part Number: SN74AXC2T245-Q1
Other Parts Discussed in Thread: SN74LV4T32-Q1, SN74LVC1G32-Q1
Hello Expert,
Our customer is looking forward following device.
Input1: 1.8V 50MHz
Input2: 3.3V 10MHz
Output: 1.8V
We could found 1:1 level shifter or OR type input logic as like as SN74LV4T32-Q1.
However, we'd like to switch 2type of different input level input as like as mux.
Is there such a device?
If there isn't it, we are planning to add switch before level translator but we'd like to optimize BOM count.
Best regards,
Kazuki Kurmaochi