This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC126A: SN74LVC126ARGYR for BT UART Application

Part Number: SN74LVC126A


Dear Sir:

Regarding the SN74LVC126ARGYR for BT UART application.

Please check the schematic connection whether it is OK and reply us ASAP.

Thanks a lot.

B.R

Vincent

Module U201 SN74LVC126ARGYR U201 SN74LVC126ARGYR  
Interface Pin Name I/O PIN NO. NAME I/O DESCRIPTION PIN NO. NAME I/O DESCRIPTION Pin Name
UART Bluetooth0 UART_CTS_J201 Input 3 1Y Output Gate 1 output 2 1A Input Gate 1 input UART_CTS
UART_RX_J201 Input 6 2Y Output Gate 2 output 5 2A Input Gate 2 input UART_RX
UART_TX_J201 Output 9 3A Input Gate 3 input 8 3Y Output Gate 3 output UART_TX
UART_RTS_J201 Output 12 4A Input Gate 4 input 11 4Y Output Gate 4 output UART_RTS