This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC8T245: SN74LVC8T245

Part Number: SN74LVC8T245


Dear Sirs

I'd like to know the capacitance value that can be directly connected to the output terminal of SN74LVC8T245.

According to the data sheet,the maximum charge/discharge current of the output is +/-50mA(continuous),but I think it is unnecesary if the capacitance value is small. 

Also,If I connect a 0.01uF cap directly to the output,do I need a current limiting resistor?

Best regards

f.kawashima