Part Number: LSF0108
Other Parts Discussed in Thread: TXU0304, LSF0102, TCA9517-Q1
Hello,
I am currently designing a test board that allows a user to hook up a MSP432's I2C and SPI lines to a device under test (DUT) at a different voltage level selected by the user. The best configuration we found seems to be using two of the LSF0108s to downconvert the 3.3V lines of the MSP432 to 1.2V, which should then allow a user to upconvert to whatever to voltage between 1.2V and 5V they want for the DUT. It seems to work in theory for I2C, but we are not confident that this should work for the SPI lines which are push-pull.
Would this usage of the LSF0108 work efficiently (up to 32 MHz) for I2C and SPI? Or will it only work for I2C?