Part Number: TXB0104
Other Parts Discussed in Thread: TXS0104E, LSF0204
Would this device work ok as I2C buffer if we use a 1K pullup on the I"C bus - as this will dominate over the 4K pulldown ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thanks for your reply.
As I want to use the same device for SPI memory buffer and I2C, the TXS104 would be OK?. I realise it has higher thresholds, the SPI wouldnt be running past 1MHZ
Yes, the TXS can be used for SPI. (The TXS has internal pull-up resistors, so you cannot use external pull-down resistors.)