Other Parts Discussed in Thread: , SN74AHCT541
Hi team,
My customer is currently using SN74LVCC4245APW but considering to move on to SN74LV541APW SN74ABT541PW for cost reduction. Could you kindly answer to the question from the customer?
[use case 1]
input: 5V
output 3.3V
Vcc=3.3V
[use case 2]
inout 3.3V
output 5V
Vcc=5V
Q: In the datasheet for SN74ABT541, it says that VOH=3V(min) (when Vcc=5V). Does this means that the output voltage varies from 3V~5.5V (This seems to be a bit wide range.)
The resciever can't handle 3V(min), so wondering if there is a situation of VOH=3V when Vcc is 5V.
Regards,
Ohashi