This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVC4T245: SN74AVC4T245DGVR drop in required

Part Number: SN74AVC4T245
Other Parts Discussed in Thread: SN74AXC4T245

Hi,

For one of our current design ;which is in production, we are using SN74AVC4T245DGVR which is out of stock (Qty required: 2.3K). 

Hence, we identified the alternate as  "SN74AVCH4T245DGVR", but as per the datasheet it says it has bus hold circuitry and an external pull up pull down should not be connected.

Can we use above alternate as a drop in? If not; can you please suggest suitable drop in replacement?

Regards,
Vidhya