Part Number: TXB0304
Other Parts Discussed in Thread: TXU0304, TXU0104, TXU0204, SN74AXC4T774
HI,
Is there a direct pin-2-pin compatible for this part with higher drive and rate?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TXB0304
Other Parts Discussed in Thread: TXU0304, TXU0104, TXU0204, SN74AXC4T774
HI,
Is there a direct pin-2-pin compatible for this part with higher drive and rate?
Thanks.
No. The TXB030x already is the higher-rate version of the TXB010x. The TXB needs a high output impedance so that other devices can override the signal voltage; decreasing the output impedance further would increase the required drive strength of external devices to more than 3 mA, which is already hard for low-voltage devices.
You have not mentioned what protocol you are using. If your signal actually are unidirectional, you can use the TXU0104/TXU0204/TXU0304.
This is for I2S with bidirectional and it's not capable of driving the audio precision digital cable.
Have you have such requirement, what do you suggest?
No, I2S can be controller or target. Here is the schematic just for the translator. Both sides go to a connector.