This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0104-Q1: 1.2V Logic Tolerance

Part Number: TXB0104-Q1

Hi,

I've noticed that the 1.2V logic VOH and VOL are listed as Typical instead of Min/Max like the rest of the logic levels. Is there a reason why it is so?

Thanks