Other Parts Discussed in Thread: BQ25121A,
Hi,
I have an application where an external switch is continuously pressed when in operation and released when not. It is powered by a battery which in turn is controlled by a BQ25121A. Unfortunately, to switch the BQ25121A active, a high signal has to change to low and then to high again. Since my external switch only manages to go from high to low, I need to have a logic element in between which pulls the line high after switching on the BW25121A. Switching it off is then done over I2C with a microcontroller.
If I use the SN74LVC1G123 to create the temporary change in voltage, I only can switch from low to high and back to low again. It is maddening but I cannot find an equivalent part which switches in an inverted way. Why does TI insist on accepting only high-low-high in their battery controller when at the same time all logic parts only switch low-high-low? And please do not tell me to add an inverter. The multivibrator should be doing the right thing from the get-go.
Regards, Peter