Part Number: SN74AVCA406
Other Parts Discussed in Thread: TXS0206A, TWL1200-Q1, TXS0206-29, TWL1200, TXS0206, TXS02612
Hello support member
# SN74AVCA406 MAX Clock speed
Checking the data sheet of SN74AVCA406, the MIN of Clock seems to be 52MHz.
Q1.
Is it correct to say that this is a typo and that the Max is 52MHz?

# level shifter for SD cards (Clock 80MHz or higher)
A customer is looking for a level shifter for SD cards with a maximum clock frequency of 80MHz or higher.
I think the level shifter for SD card is the following product.
(SN74AVCA406)
TXS0206A
TWL1200-Q1
TXS0206-29
TWL1200
TXS0206
TXS02612
These products do not work a clock of 80MHz or higher.
Q2.
Is it correct to understand that TI does not have a level shifter for SD cards with a clock of 80MHz or higher?
Best Regards,