Part Number: SN74LVC2T45
Other Parts Discussed in Thread: SN74LXC2T45
Hello,
I am designing a FMC board for the communication between two main boards. The FMC board will be connected to both master and slave boards and two FMC will be connected through Cat5 ethernet cable. Master is foreseen to control 3 slaves. All slaves are controlled through common SPI pins and they differ on Chip Select. I am forced to use SN74LVC2T45 for configurable voltage level translation between Master and Slave Boards. The distance between two boards will be around 10 meters. Can you please provide information about the capacitive load capacity of SN74LVC2T45 so that I can try to figure out maximum distance I can transmit my signals through Cat5 ethernet cables. I am aware that 10 meters is far away. Depending on the maximum distance achieved with SN74LVC2T45, I am planning to design an intermediate repeater board between two FMC.

Regards,
Selim