Other Parts Discussed in Thread: TXB0304
Hi team,
is there any level shifter recomendation for the Quad-SPI application?
Reqiurment:
Max Clock: 100Mhz
1.8V to 3.3V/ auto-bi-directional
and Host CPU SPI spec TCLH (clock high time)/ TCLL (clock low time) Min is 3.9ns,
so need low propagation delay for better setup time margin, please note it.
BTW, we find the TXB0304 "Data rate" (max) (MBps) is 140, so it can suppot the max "clock" 100Mhz as well?
please help to clarify it.
Thanks