Part Number: CD4013B
Dear Technical Support, attached is CD4013B datasheet and P.4 of the related datasheet, the circled area of P.4 shows that the " Clock Input Frequency " related data, and it listed the MIN. & TYP. data values,
but not listed the MAX data value,
I am wondering if there is a mistake on this data values, I think the MAX data should not be left open, the left-open data should be the MIN data instead,
It is because for this kind of Logic Devices, there should be a MAX. Clock Input Frequency limit value, but should have no MIN. Clock Input Frequency limit, and this is because if the Clock Input Frequency is too high, then there is a possibility the data cannot recognized and shown correctly at the output of the device,
Not sure if I am right on this? Please let me know if I am wrong and why I am wrong if convenient.
Look forward to hearing from you when convenient.
Thanks
yenwu lo