This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC244A: SN74LVC244ARWPR Ibis Model

Part Number: SN74LVC244A


I got the Ibis model for SN74LVC244A, but in that package I couldn't see SN74LVC244ARWPR (Which is having X1QFN Package)

  • Hi Haritha,

    SN74LVC244A is the only device which we offer in the X1QFN package type and I'm not sure there are any plans to develop model for this package specifically.

    I would recommend just simulating using the VQFN package. There should not be much of a difference between the two.

    Best,

    Malcolm