This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AXC4T774: VCCA and VCCB supply restriction

Part Number: SN74AXC4T774
Other Parts Discussed in Thread: TCA9416,

Hi, can you confirm there's no supply restriction for SN74AXC4T774 and TCA9416 ? 

I can put VCCA and VCCB as 3.3V without issue and VCCA can be greater or smaller than VCCB, correct?

Thanks

  • Hey Ken,

    Yes that is correct, so long as it is within the bounded region in the recommended operating conditions. Please note that the AXC4T774 is not compatible with I2C applications and, while it does provide buffering, it is not the same "buffering" function that is known in I2C buffers.

    Regards,

    Jack