Part Number: SN54HC595
How do I test out shift register? I have two series of four (4) shift registers connected in row. Four SN54HC595 for SIPO and four (4) 54HC166 for PISO.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN54HC595
How do I test out shift register? I have two series of four (4) shift registers connected in row. Four SN54HC595 for SIPO and four (4) 54HC166 for PISO.
Hi Viraj,
To test SIPO devices:
To test PISO devices:
Sorry that this is not an extremely detailed description, but I recommend that you just read through the datasheet, especially the detailed description sections, as well as the recommended operating conditions. In general, make sure all inputs don't go above VCC or below 0 V and you should be fine.