Part Number: SN74LVC2G07
Other Parts Discussed in Thread: TXU0102, SN74LVC2G34
Hi Team,
can the SN74LVC2G07DRY be used to buffer two clock lines that are 5 V level and to convert them to 3.3 V as well?
What is the skew between the two devices? E.g., if one channel gives 2 ns delay, within which range can I expect the other channel to be?
Or would you recommend another solution for this, i.e: LMK1C110x
BR,
Stefan