Other Parts Discussed in Thread: TINA-TI
Hello,
in our new design I use SN74LXC8T245QPWRQ1
for voltage translation 3.3V -> 5V. The circuit drives an external component (no design of our own).
The external component has parallel 16 bit interface, altogether there are 3 IC working in parallel to handle the bus.
There is heavy ringing on the output lines, I would try to limit the output driving strength.
Simulating the situation would help.
The question is: How can I make use of the provided IBIS model "SN74LXC8T245-Q1.ibs" (delivered in scem783a.zip)
Is it possible to import the IBIS file into TINA-TI V9 (9.3.200.277 SF-TI)?
Other options to see transient response of output pins?
Thank you & greetings
  michael