Other Parts Discussed in Thread: TXU0304, TXU0104, TXU0204
Hi,
I have the circuit in the following schematic. With an FT4232 connected to the 3.3V side of the LSF0204RUT and headers on the 1.8V side. The goal for this board is to go from 3.3V logic to 1.8V. There is nothing connected to the 1.8V rail aside from the LSF0204RUT and the TLV70218.

When I don't have the LSF0204RUT in the board I measure about 1.9V out of the TLV70218.
However when I place the LSF0204RUT in the board I measure around 2.3V on the 1.8V rail and can see 2.3V logic. Is there a reason why the LSF0204RUT is pulling the 1.8V rail up?
Best
Camilo