Hi,
I was thinking of using this IC as a discrete buffer for two synchronous clocks. The issue I'm running into is finding information on the minimum propagation delay for operating VCCA & VCCB at 3.3V. Is this specification available?
I'm having difficulty finding comparable ICs with tight propagation delays. In my application I need a propagation min/max delay difference less than 1.62nS. If it turns out this IC's min spec causes a prop difference delay greater than 1.62nS are their other discrete devices available that are available?
Regards,
Lee
Electrical Engineer