This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2G07: Output Capacitance

Part Number: SN74LVC2G07

Hi,

For the part  SN74LVC2G07DCKT, I am looking for the output capacitance.

The datasheet provides the Ci which is 3.5pF.

But it doesn't provide the output pin + driver capacitance when a steady 3.3V is driven out.

Is it a data you would have ?

Thanks.