Part Number: LSF0204
Other Parts Discussed in Thread: TXU0202,
Hello,
we need to use this transceiver as Push-pull.
how this can be used?
Regards,
Sudharshana
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The LSF can accept push/pull signals at its inputs. It always outputs open-drain signals. (And it is not a transceiver; it's a passive switch and does not buffer the signals.)
What protocol are you using? What is the actual problem you're trying to solve?
Hi
We are interfacing SC206 IC UART TX/RX ports to LSF with 1.8V supply and output is interfaced without pull up as it has mentioned as push-pull to L76 gps IC.
Regards,
Sudharshana
The best choice for this application would be the TXU0202.
The LSF0204 can be used, but only if the output on the high-voltage side has a pull-up resistor.