Other Parts Discussed in Thread: SN74LV1T125, SN74AHCT1G125
Dear Team,
I have a question about SN74LVC2G125:
OE is L, VCC=5V, when the A port is 3.3V high level, is the Y port a 5V high level?
Many Thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team,
I have a question about SN74LVC2G125:
OE is L, VCC=5V, when the A port is 3.3V high level, is the Y port a 5V high level?
Many Thanks,
Jimmy
Hi Jimmy,
No. At VCC = 5V, the VIH min is 0.7*VCC = 3.5V. A is in between the VIH min and VIL max and can potentially damage the device; the Y port MIGHT register as a logic high but this performance is dubious and not guaranteed.
Best,
Malcolm