This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AXC4T774: IBIS Model Question

Part Number: SN74AXC4T774

My Customer is using SN74AXC4T774RSV level shifter IBIS model in a Signal Integrity simulation. The IBIS model was downloaded from TI website.

 

"In our design, we need 3.3v and 1.2v two types IOs. However, in this level shifter ibis model, there are no 1.2v models( see the screen capture below).    Does this IBIS model work with 1.2v IO which means the power rail is 1.2v, but with the 1.8v IO model/1.8v digital input model?

 

Can TI provide the level shifter IBIS model with an IO model for 1.2v input and 3.3v output, and 1.2v digital input model?"

 Please advise :)