Other Parts Discussed in Thread: TXU0202
Hello expert,
Does A1 A2 B1 B2 of SN74AXC2T45 have internal pull-up?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello expert,
Does A1 A2 B1 B2 of SN74AXC2T45 have internal pull-up?
Hi Clemens Ladisch,
I have another question.
The DIR of SN74AXC2T45 changes the A1 A2 input or output mode at the same time.
Customers need more flexible direction choices, for example:
A1 is in, B1 is out
A2 is out, B2 is in
Does TI has the products, which input and output direction of the two channels can be changed individually, or fixed as A1 input, A2 output.