Dear TI team,
I am using SN74ACT244PWR as buffer for PWM signal which is up to 200 kHz. I see that there is slight overshoot from control board PWM signal (30% overshoot on 3.3 V PWM signal) which is input to buffer. I am observing that similar overshoot (25% on 5 V PWM signal) at the output of buffer.
Kindly let me know if there is a possibility to avoid this noise transmission.
Thanks,
Shritesh