Part Number: SN74AUC17
您好,请问:
SN74AUC17这颗芯片,VCC电压写的是最大2.7V,极限电压写的是3.6V,芯片VCC能不能采用3.3V供电?如果采用3.3V供电将有何影响,谢谢

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When you try to power it with 3.3 V, the absolute maximum ratings are not exceeded, so it will not be permanently damaged. But it does exceed the recommended operating conditions, so the electrical characteristics, or even correct operation, are no longer guaranteed.