Other Parts Discussed in Thread: TXU0304
Hello,
The advice on level sifter TXS0108EPWR.
Is it suitable for SPI application?
If it is not, what’s TI suggestion?
Best Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gary,
Please help see section 1 of Voltage Translation Application Quick Reference, with TXU0304 as an example for SPI, thanks.
Best Regards,
Michael.
Hello Michael,
Thank you for the suggestion. So, TXS0108EPWR cannot be used for SPI?
Best Regards
Hi Gary,
TXS can be used, but not the most suitable. Due to limitations such as the datasheet's section 9.3.3 i.e fixed directional devices such as TXU are best recommended for fixed directional signals such as SPI.
Hence, if the datasheet's considerations are of no concerns, then it will work just fine, thanks.
Best Regards,
Michael.