This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AXC8T245: Device-to-Device Skew

Part Number: SN74AXC8T245
Other Parts Discussed in Thread: DAC900, , TXV0108-Q1, TXV0106-Q1

Hi team,

When I use multiple SN74AXC8T245s, what is the skew between the devices?

The system has 11 bits of clock and data, so I am concerning. 

(I understood from previous E2E that the maximum skew in the device is 1ns. )

[System]

FPGA(1.8V) - SN74AXC8T245 - DAC900(3.3V)

Best regards,

Goto