Other Parts Discussed in Thread: LSF0102
I am goint to use the device LSF0102QDCURQ1 as I2C voltage level translator, from a 3,3 V I2C bus (VCCB) to a 1,8V I2C bus (VCCA) and viceversa. I was checking for compatibility with the other devices (on the same bus) voltage levels and I wasn't able to find out the input threshold of the LSF0102. So my question is how to ind out the:
- max input low level B and A side
- min input high level B and A side