Part Number: SN74LVC1G17
If VCC = 0V and A = 0V will Y sink current? In our circuit is seems to do that. This is not a problem for the circuitry; is 10mA current sink in this condition safe for SN74LVC1G17DRLR?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74LVC1G17
If VCC = 0V and A = 0V will Y sink current? In our circuit is seems to do that. This is not a problem for the circuitry; is 10mA current sink in this condition safe for SN74LVC1G17DRLR?
Section 8.1 of the datasheet says:
This device is fully specified for partial-power-down applications using Ioff. The Ioff circuitry disables the outputs, preventing damaging current backflow through the device when it is powered down.
Can you confirm that the voltage at the VCC pin is measured to be 0 V?
Below the supply voltage minimum limit of 1.5 V, there are no guarantees. But it is indeed possible that the device is still active, and that A = 0 V will drive the output low.
The absolute maximum ratings allow a sink current of 10 mA.