This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

sn74lvc2g07 versus sn74lvc3g07.

Other Parts Discussed in Thread: SN74LVC2G07, SN74LVC3G07

Hi, I am interesting in a buffer/driver with open-drain outputs. I've read  the datasheet sn74lvc2g07 (2 buffers), on the page  3 showns the function table [Table A]. I've also read the datasheet sn74lvc3g07(similar to sn74lvc2g07 but with 3 buffers) on the page 2 the function table [Table B], I've seen a difference in these tables, in the table A when the input is H, the output is Z but in the table B when the input is H, the output is H. Is it ok?

If the answer is correct, then Are these devices different?

Thank you so much.