Other Parts Discussed in Thread: UCC37324, UCC27516, TLC3704
Hello
I am looking for a Low to High ( 3.3 V to 15 V ) Translator with at least 10 mA Source & Sink
capability for Interface between our DSP and IGBT Drivers.
Two / Four or Six Channels are what I am looking for
Because of Source / Sink requirements, Open Coll Darlingtons or Op Drain is not an option.
CD4504 seems one option , but the Data Sheet is not too comfortable with 3.3 V to 15 V,
5 to 15 it seems fine.
Can I use that to comfortably translate the 3.3 V DSP Signals to +15 V ?
Best Regards
Varun