This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0204: Pass transistor current

Part Number: LSF0204

Hi, 

I have some questions about LSF0204 level shifter.

In datasheet, recommended pass transistor current is 64mA. 

And, pull-up resistor should limit the current through the pass transistor when it is in the ON state to about 15mA.

Does it mean ON state pass transistor current is 15mA(typ) and 64mA(max) ?