Hi,
What's the input and output impedance of this level translator?
How would I go about matching this translator to (say) a 50-ohm trace. Are there any guidelines on what kind of termination to use on the inputs and outputs?
Thanks,
Navneet
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
What's the input and output impedance of this level translator?
How would I go about matching this translator to (say) a 50-ohm trace. Are there any guidelines on what kind of termination to use on the inputs and outputs?
Thanks,
Navneet
The input impedance is approximately infinite, see [FAQ] What is the impedance of the device's input pin? Is it CMOS or bipolar device?
The output impedance is somewhere between about 10 Ω and 75 Ω, depending on the output supply voltage; see [FAQ] What is the output voltage (VOH or VOL) when the output current is X or the supply voltage is Y?
To terminate a trace, you would typically use a source termination resistor; see [FAQ] What happens when I connect a logic device's output to a 50 ohm transmission line?