Part Number: SN74LVC1G06
Other Parts Discussed in Thread: TPS3422
Hello! I'm using SN74LVC1G06DBVR for the delayed reset of my STM32. I expected that the reset signal would be triggered after more than 10-11 seconds. According to the datasheet, I anticipated that the threshold would be a 2V input signal. However, the reset signal is triggered at the level of 1.240 - 1.245V, some times 1.65 resulting in the reset occurring after 6.5 seconds. I could increase the capacitance up to 33uF, but I'm unsure which threshold value I should consider.