Part Number: TXB0104-Q1
Other Parts Discussed in Thread: TXS0104E-Q1, TXU0304-Q1, TXU0104-Q1, TXU0204-Q1, TXB0104, TXS0104E
Hi team,
As you can see, we have the following connection method. We used TXB0104-Q1.
There are no pull-up and pull-down resistors inside the SOC. And there are no pull-up and pull-down resistors throughout the entire sequence.
The signal is a low-rate UART signal.

Is this connection method feasible?
We found a strange phenomenon. After passing the first TXB0104-Q1, the data appeared at an intermediate level, and the UART recognized garbled characters.
But when we replaced all the TXB0104-Q1 in the middle with TXS0104E-Q1, this problem did not occur.
Can you explain this phenomenon? I think TXB0104-Q1 should be fine too. Do you have any suggestions if we are too late to replace the TXB0104-Q1?
Thanks
Xiaoxiang