This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUP1G125: Max V_OL for Vcc=1.1V?

Genius 12865 points
Part Number: SN74AUP1G125


Hello Team,

the data sheet specifies a max V_OL of 100mV at I_OL of 20µA and Vcc=0.8V ... 3.6V.

Can you confirm that V_OL,max will be 50mV at Vcc=1.8V?

Will V_OL be reduced to 50mV if I_OL is just 10µA? 

Can we expect a max V_OL of less than 83mV at Vcc=1.1V and I_OL<=5uA?

Thank you and Best Regards, Hans